SKIP TO MAIN CONTENT

Primer centro de datos de Francia alimentado con HVO, gracias al conocimiento experto de Rehlko.

The Digital Realty PAR8 centre, situated a stone's throw away from Paris, necessitates unparalled power redundancy to cater to the increasing demands of the data centre sector.

With the support of Rehlko's auxiliary generators, this state-of-the-art facility is capable of operating at peak capacity for an impressive 72 hours, utilising environmentally friendly, renewable hydrotreated vegetable oil (HVO) as fuel.

Delve deeper into how Rehlko and Digital Realty are joining forces to provide data center clients with cutting-edge, eco-conscious solutions!



Take a look at Rehlko's ability to handle large-scale data center projects.


  • Complete installation and comissioning by Rehlko

  • 36 x 2200 kVA containerized generators already installed

  • 2nd part of the building under construction and future installation of 36 more generators

  • 131 MW capacity

  • All generators run on HVO