Por qué elegir repuestos originales Kohler?
The Digital Realty PAR8 centre, situated a stone's throw away from Paris, necessitates unparalled power redundancy to cater to the increasing demands of the data centre sector.
With the support of Rehlko's auxiliary generators, this state-of-the-art facility is capable of operating at peak capacity for an impressive 72 hours, utilising environmentally friendly, renewable hydrotreated vegetable oil (HVO) as fuel.
Delve deeper into how Rehlko and Digital Realty are joining forces to provide data center clients with cutting-edge, eco-conscious solutions!
Take a look at Rehlko's ability to handle large-scale data center projects.
Complete installation and comissioning by Rehlko
36 x 2200 kVA containerized generators already installed
2nd part of the building under construction and future installation of 36 more generators
131 MW capacity
All generators run on HVO