Kohler Launches Mobile Paralleling Box
Kohler Power Systems is launching a new Mobile Paralleling Box, which delivers cutting-edge flexibility by allowing users to combine different sized generators with different fuel types. The new paralleling box, specifically designed for use with Kohler’s gaseous and diesel mobile generator line, was officially introduced during the recent 2015 PGA Championship at Whistling Straits.
“We’re excited to introduce this new technology and proud to have launched it during the PGA Championship,” said Anne Feudner, product manager for Kohler Power Systems. “This new product will bring unmatched flexibility and a new level of customization to a wide variety of applications – including large scale, world-renowned events like the PGA golf tournament.”
Mix and Match
The new Mobile Paralleling Box, along with a fleet of Kohler generators, allows users to mix and match different size generators to meet job requirements. Four of the new boxes can be used to parallel as many as eight generators. The Kohler Decision-Maker 3500 digital controller, which is standard on all Kohler gaseous and Tier 4 Final diesel mobile generators, provides the paralleling intelligence and network communications for remote monitoring.
“Any Kohler mobile generator with the Decision-Maker 3500 digital controller will work with the Mobile Paralleling Box,” Feudner said.
The digital controller along with the new Mobile Paralleling Box makes it possible to parallel generators for applications such as using multiple smaller units to replace a larger generator, providing redundancy to a primary generator in support of critical loads, meeting system capacity demands when one generator is inadequate, or managing generators to be sequenced on or off in a predetermined order based on system output.
One Size Fits All
The new system uses contactors to connect to the bus and eliminates the need for installing or investing in motorized breakers on generators that may never be used in a parallel application. Each contactor is rated at 1,000 amps – different sized generators can parallel as long as each unit’s output is less than 1,000 amps.
“The advantage of the new paralleling system is that it removes the need to size circuit breakers to specific generator output,” Feudner said.
Color-coded camlocks for input and output feeds make the new box easy to setup and maintain while unused camlock connectors are protected with lockable security bars. The system also includes two 25-foot control cables as well as lockable storage for control cables. During the PGA Championship, the Mobile Paralleling Box from Kohler Power Systems was used to provide power redundancy for Kohler Co. hospitality tents. A Kohler 175REOZT4 Tier 4 Final diesel unit was used as the primary power source and a Kohler 125REZGT – an EPA-certified gaseous unit that runs on LP – served as a secondary power source.
Advanced Digital Controller
Paralleling intelligence is incorporated into the Kohler Decision-Maker 3500 digital controller, which provides system monitoring and diagnostics while also offering a user-friendly display. The advanced digital controller uses a patented hybrid voltage regulator and unique software logic to manage alternator thermal overload protection features that normally require additional hardware. Paralleling functions featured on the controller include:
Bus sensing for accurate metering and control
First-on logic – starts all generators to allow the first generator to reach rated voltage to close to the bus
Synchronizing adjusts other generators’ engine speed and voltage to allow them to connect to the bus
External-controlled load sharing via analog bias signals
Load management to ensure the generators are not overloaded
The Kohler Difference
Kohler offers a number of support services that will give rental companies and other users an edge on the competition, including a premium three-year limited warranty and Custom-Engineered Specials to design a mobile generator that fits every job perfectly. From custom paint and decals to receptacle connectors and fuel tank capacity, Kohler makes it easy to get exactly what a customer needs. Kohler’s global service and support network, with more than 800 locations worldwide, also provides aftermarket support services to guarantee the satisfaction of their mobile generators and other products.
About Kohler Power Systems
Kohler Power Systems, a division of Kohler Co., provides complete power systems, including generators (residential, industrial, mobile, portable, and marine), automatic transfer switches, paralleling switchgear, monitoring controls, and accessories for emergency, prime power and energy-management applications. Kohler Power Systems has delivered energy solutions for markets worldwide since 1920. For more information, visit www.kohlerpower.com.
About Kohler Co.
Founded in 1873 and headquartered in Kohler, Wis., Kohler Co. is one of America’s oldest and largest privately held companies comprised of more than 30,000 associates. With more than 50 manufacturing locations worldwide, Kohler is a global leader in the manufacture of kitchen and bath products; engines and power systems; premier furniture, cabinetry and tile; and owner/operator of two of the world’s finest five-star hospitality and golf resort destinations in Kohler and St Andrews, Scotland. For more details, please visit Kohler.com.
Media Inquiries
Erin McMahon
Account Director
erin.mcmahon@publitek.com
+1 630-962-7535