Skip to main content

Case Study

Case Study: Agriculture

Meunerie Saint-Hugues | Saint-Hugues, Québec

Two generators in different sizes, small and big outside a building.

At a Glance

CUSTOMER
Meunerie Saint-Hugues

LOCATION
Saint-Hugues, Québec

INDUSTRY
Agriculture

CHALENGE
Provide emergency standby power for a continuous process operation to avoid unplanned outages that would otherwise affect livestock health

SOLUTIONS

  • Three diesel generators with onboard paralleling

  • Closed-transition transfer switch and weather-protective enclosures

Note: The products shown were installed under the KOHLER brand.

Background

Meunerie Saint-Hugues, a Québec-based agricultural processing facility, required reliable emergency standby power to prevent unplanned outages that could impact livestock health and disrupt operations. The facility needed a solution that could be deployed quickly and fit within the available mechanical building space.

Initially, a single 1500 kW genset was considered, but its size and related equipment would have required additional site preparation and increased installation costs. Project timing was also a major factor—Meunerie Saint-Hugues sought a supplier who could deliver and commission the solution in the shortest possible timeframe.

Challenge

The facility needed:

  • Continuous emergency power without interruptions to production

  • A solution that met space, cost, and redundancy requirements

  • Quick delivery and installation ahead of the holiday season

  • Reliable operation even in Québec’s harsh winter weather

Case Study G18-516 - Two gensets outside Meunerie Saint-Hugues facility

Rehlko diesel-powered generators with onboard paralleling and integral subbase fuel tanks

Case Study G18-516 - ATS St-Hugues - ATS outside the power room

Rehlko closed-transition transfer switch

View of Meunerie with parking lot

Meunerie Saint-Hugues facility

Solution

To meet these constraints, Meunerie Saint-Hugues partnered with trusted supplier Drumco Énergie. Drumco’s agricultural sales representative, Carrol Allen, and technical director, David Vigeant, recommended a Rehlko emergency standby solution.

The solution included:

  • Three Rehlko diesel generators with onboard paralleling, each rated 500 kW standby

  • Rehlko APM603 generator controllers for on-board paralleling, ensuring sufficient power coverage during weekday outages

  • Rehlko CSA-Listed weather-protective enclosures with block heaters and multiple access doors for easy service

  • Subbase fuel tanks with secondary containment and UV-resistant coating for faster installation and long-term reliability

  • Rehlko KCS-ANTA-3000S closed-transition transfer switch for fast, automatic transitions between grid and standby power

The multiple genset configuration provided redundancy, allowing one generator to undergo maintenance while others remained in service. This approach also accommodated variable production schedules, avoiding the need for an oversized 1500 kW unit.

The solution for Meunerie Saint-Hugues includes:

Three Rehlko diesel generators with onboard paralleling, integrated subbase fuel tanks, and automatic transfer switches, providing reliable standby power within a compact facility footprint.

Results

The integrated emergency standby power system was delivered, installed, and commissioned quickly, functioning flawlessly during multiple utility outages.

“Drumco Énergie is very sensitive to the particular needs of the agricultural market in Québec,” said Carrol Allen, Drumco Énergie’s agricultural sales representative. “Reliability of the emergency generator can mean the difference between life and death of the animals. We take great pride in supplying reliable equipment and backing it up with 24/7 emergency service.”

*Rehlko is a global leader in energy resilience delivering innovative energy solutions critical to sustain and improve life across home energy, industrial energy systems, and powertrain technologies, by delivering control, resilience and innovation.

Latest Case Studies

Health City Hospital at Camana Bay.

Case Study

Healthcare

Rehlko provided a backup power system to protect critical equipment and maintain essential healthcare services during utility disruptions.

Close up image of a hydrogen fuel cell system with the Rehlko logo

Case Study

Healthcare

Fort Hayes State University

Case Study

Education

Learn why this university in Kansas trusts in a Rehlko Power System.

Store front of Benny and Co Restaurant.

Case Study

Hospitality

Learn about integrated emergency standby power solutions.

Man running inside a data center.

Keep your Business Running

Rehlko Power Systems has delivered energy solutions for markets worldwide since 1920.

Contact your Rehlko representative for more information.