Skip to main content

eFRAMETM Enclosures: Built for Critical Applications and Designed for Ease

Backup Power for Industrial Use

How supporting continuity in mission-critical sectors enhance the installation and servicing of generators

eFRAME ™ Enclosures, Direct From Rehlko.

Access to reliable and sustainable back-up power from generators is critical to operations in places like data centers, water utility plants, and healthcare facilities. When the grid goes down, these tried and trusted solutions come online in a matter of seconds, providing the energy continuity needed to keep vital systems running…

In many ways, generators are the unsung heroes of mission-critical environments, sitting unobtrusively in the background, ready to go. Yet, this state of preparedness requires foresight and planning. Generators must be housed and maintained in optimal conditions to ensure they perform at the highest level.

What is the best way to create controlled conditions to deliver power excellence on demand? The answer comes with locating generators in rugged, yet easily accessible enclosures built explicitly for mission-critical applications. These enclosures cover and protect the generator from outside elements such as; rain, snow and high winds, animal intrusion, and unwanted entry.

Notably, the latest generation of walk-in enclosures has been meticulously designed to provide operational advantages across the lifecycle. This approach includes design for ease of installation and servicing - which saves time, money and effort over the long term.

Introducing eFRAME enclosures from Rehlko

Let’s delve deeper into the advanced engineering of Rehlko eFRAME enclosures, designed to house the KD Series in configurations 2 MW - 4 MW. By examining their features, we can gain a clearer understanding of the installation, maintenance, and operational benefits they offer.

At a headline level in terms of construction, a customized and modular approach to the design ensures that these walk-in enclosures can be configured explicitly for any mission-critical applications. The enclosures are made of durable all-aluminium construction and a fade/scratch/corrosion-resistant exterior.

The eFRAME enclosures can be designed to provide significant space around the generator for direct access, enabling maintenance teams to carry out servicing in a comfortable and accessible environment. For example, it provides easy access to the entire generator inclusive of the engine and radiator without disconnection, promoting rapid troubleshooting. They also come with an easy-to-remove single-piece roof, making the replacement or service for any generator component straightforward. These design characteristics help reduce service costs and downtime across the lifecycle.

How generator enclosures are built to last

Reliability is also crucial. Receiving the UL 2200 FTPP certification for construction, the eFRAME has been designed to meet and withstand over a 135-mph wind load rating. Meanwhile, Computational Fluid Dynamic tools review the enclosure airflow to ensure generators operate efficiently in the most demanding environments. Each enclosure goes through vigorous testing and approval. Additionally, the enclosure is IBC-certified for site-specific use, and its sub-base tank meets UL142, cUL, and state-specific requirements.

Taking a total system approach also delivers significant end-user benefits. The eFRAME enclosures are specifically geared to accommodate Rehlko generators and every unit is designed, built and tested in Rehlko’s Wisconsin factory. This single-source process provides consistency in production quality and allows for shortened lead times. They are also designed for effortless installation, saving time and resources on-site.

Built for critical applications and designed for ease

In short, the eFRAME enclosures from Rehlko makes life easier for mission-critical end users. They can be designed to meet individual requirements, built to consistent standards, and installed quickly and easily. Their design characteristics encourage streamlined service and maintenance throughout the years. This enables flexible and reliable power when needed – ultimately offering peace of mind.

Rehlko enclosure with the lid lifted to see modular construction inside

Built to Perform. Engineered to Endure.

Rehlko walk-in enclosures deliver smarter access, simplified service, and protection that lasts.

Latest blog posts

Grey building with lights on cloudy day

Blog

NFPA 110: Why It Matters for Backup Power

Male professional touching a panel

Blog

ATS: The Unsung Hero of Resilient Power Systems

Rehlko Parallel Switch Gear

Blog

Understanding the Benefits of Paralleled Standby Generators

Male professional working on a generator inside a building

Blog

Proactive Generator Maintenance: Why It Matters

Man running inside a data center.

Keep your Business Running

Rehlko Power Systems has delivered energy solutions for markets worldwide since 1920.

Contact your Rehlko representative for more information.